AXIS#.MOTOR.ICONT

Description

This parameter is the motor continuous current.


  • This parameter is required to be configured for all motor types.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

0.1 to 500

Default Value

1

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.ICONT

500bh

10h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6204

1

6204 (0x183c)

AXIS1.MOTOR.ICONT

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MOTOR.ICONT

6204

Float

Read Only

-